When designing hot water systems the water temperature, water retention time, pipe material and making way for regular system maintenance is of great importance in order to prevent microbacterial growth.
Legionnaires' disease is a serious lung disease which is caused by breathing in aerosols infected with the bacteria Legionella Pneumophila. Of those who are infected up to 30% will die.
A level sensor is a device that measures the water level.
The life cycle cost of a pump system is the total cost of all system components over their lifetime. This is typically 10 - 20 years.
A liquid subcooler is fitted in a cooling plant in order to increase the performance of the evaporator. It lowers the refrigerant inlet temperature to the evaporator.
Listed and approved components for fire protection are those that have been tested and certified by accredited laboratories- for example; the fire pump-end, control-panel, flow-meter etc. These components are typically published by the organization via webpage or CD’s etc.
LON is an open network technology which is mainly used in building automation. The name LON is short for "Local Operating Network". It is an event-based technology that supports a variety of physical network standards, making it ideal for use on all automation levels.
Magnets are used to drive the shaft and impellers in this product group within the CR product family. , There is no physical connection between the pump and motor, allowing it to be hermetically sealed against leaks.
In heating and air conditioning systems, water must be distributed from the supply system to the point of consumption. This is done by means of main pumps.
The calculation of the life cycle cost of a pump system includes the total cost of maintaining and repairing the system over its lifetime.