Natural refrigerants

Natural refrigerants have no, or an insignificant, impact on the ozone layer and greenhouse effect. They are widely used in smaller applications, such as heating pumps, small chillers, and commercial systems.

 

For quite some years, natural refrigerants have been the proper thing to use in larger industrial cooling systems within food and beverage industries for both production and storage – especially NH3 and CO2 which are used for industrial purposes with low temperatures.
Due to the increased focus on the harmful effect of refrigerants on the environment, the natural refrigerants have experienced a renaissance. Today they are widely used in smaller applications, such as heating pumps, small chillers, and commercial systems – with the HC types especially common in smaller systems. At present, the most common of these refrigerants are R600a and R717. The typological classification HC stands for HydroCarbon and states the content of atoms in the molecules.
 
Natural refrigerants have no, or an insignificant, impact on the ozone layer and greenhouse effect. Therefore, everyone is working intensively to incorporate natural refrigerants in the cooling systems of tomorrow.
 
Pure substances
R170              Ethan
R290              Prophane
R600a            Isobutane
R717              Ammonia
R718              Water
R729              Air
R744              Carbon Dioxide
R1270            Propylene
 
Mixtures
ODP (Ozone Depletion Potential) states the refrigerants impact on the greenhouse effect compared to a R12 value of 1.0.
 
GWP (Global Warming Potential) states the refrigerants impact on the greenhouse effect compared to a Carbon Dioxide value of 1.0.