In any thermal heat exchange process, a mixture of two energy flows will result in a new stage or phase called the balance point. Here, a common temperature, humidity or enthalpy is reached.
Balancing of heating and cooling systems is performed to ensure that the correct amount of water is present at all consumption points. Balancing is carried out by building balancing valves into the system, thereby adding adjustable resistance.
During commissioning of heating and cooling systems, hydraulic balance is often achieved using balancing valves; static or dynamic.
Building information modeling is an innovative method to seamlessly bridge communication within architecture, engineering and construction industries. With BIM, architects and engineers efficiently generate and exchange information, create digital representations of all stages of the building process, and simulate real-world performance.
Biocide is a chemical added to the water within evaporative applications such as condensers and cooling towers.
Biocide is a chemical added to the make-up water for evaporative applications such as condensers and cooling towers.
Biofilm refers to a population of various micro-organisms trapped in a layer of slime and organic matter that attaches itself to the surfaces of pumps, pipes, walls etc.
Black water is sewage water for industrial and waste water applications. Pump types used are submersible non clog, dry pit non clog, and non clog wet pit column pumps.
A Building Management System (BMS) is an integrated data network and control system for automation, monitoring and control of HVAC, lighting and other functions in a building.